You are here: Understanding KAS > Motion Concepts > Pipe Network Concept > Executing Motion

Executing Motion

Two types of Pipe Blocks are used to command motion in a Pipe Network: Axis block and Input block.

In the following example, executing MLAxisMoveVel, MLAxisAbs and MLAxisRel Functions can be used to cause motion on a particular axis. Whereas MLMstRun, MLMstAbs and MLMstRel functions cause motion on Axis1, Axis2 and Axis3.

For information on error management, Error Management.

For explanations on restarting the motion, refer to Restarting Motion

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™